AXIS#.PL.KITHRESH

Description

This parameter sets the velocity command threshold when the position loop integrator turns off.

If velocity command is less than AXIS#.PL.KITHRESH, the position loop integrator will be active. If the velocity command exceeds AXIS#.PL.KITHRESH the position loop integrator is disabled (it will act as if AXIS#.PL.KI = 0).

Usage

As a general rule, AXIS#.PL.KI should not be used at the same time as AXIS#.VL.KI , the two integrators will oppose each other and likely cause undesirable results, sometimes a runaway. Using AXIS#.PL.KITHRESH in conjunction with AXIS#.VL.KIMODE the user can specify operating conditions to switch between integrators based on machine operation.

It often makes sense to use the velocity integrator during a move, but as the motion comes to an end, to switch back to the position integrator for fine positioning.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Velocity (See AXIS#.UNIT.VROTARY AXIS#.UNIT.VLINEAR )

Range

0 to AXIS#.VL.LIMITP

Default Value

AXIS#.VL.LIMITP

Data Type

Float
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
AXIS1.PL.KITHRESH

500ch

0eh

Signed32

Velocity

-

Read/Write

No

AXIS2.PL.KITHRESH

510ch

0eh

Signed32

Velocity

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.PL.KITHRESH

5916

171C

Signed32

Read/Write

Velocity

AXIS2.PL.KITHRESH

71452

1171

Signed32

Read/Write

Velocity

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.PL.KITHRESH

5916

Float

Read/Write

Velocity